Olemme

Virhe occursed kun lähettää viestin, yritä myöhemmin uudelleen

Kysymyksenne

Hard Facts about effect of climatge in swine.jpg

Hard facts about effect of climate control in swine

Yes, we have hard facts, which prove the importance of advanced climate to improve productivity in 4 legs industries!

Mortality

When a small pig is born, one of the most important parameters is to secure the right climate conditions. If this is not done, there is a risk that it will die, lose weight or not get the first important raw milk from the sow.

A PhD study from Denmark shows that a too cold climate for new born pigs is the primary reason for mortality in the farrowing units. A dead small pig has negative impact on the farmer’s economy as he still has to give the sow the same amount of feed, use the same pen area, use the same electricity etc.

Optimal climate in the farrowing unit is essential since the piglets and the sow want different temperatures and if it is too hot for the sow, she will produce less milk.

Survival of one extra pig per sow has an economic value of around 33 Euro (244 dkr), depending of feed prices, meat prices, electricity cost, housing design and a lot of other parameters (prices in Denmark August 2016).

When the pigs get older they produce a lot of heat. This heat is removed by advanced ventilation systems. If the ventilation system for some reason breaks down the pigs will die after 20-40 minutes depending on age of pigs and housing design. Therefore it is essential to have reliable ventilation and alarm system. Maybe people outside the industry think “Why don´t they just keep the pigs outdoor”. Here the answer is that we cannot feed the world if all animals were outdoor. That would simply lead to too much uncontrolled pollution into the nature and not enough space. Also from a biosecurity point of view it is better to have the pigs indoor in controlled environment. Also in countries where the out-door temperature is high it is better for productivity to have the pigs indoor in buildings with advanced climate system.

Facts

  • The primary reason for mortality among new born pigs is the climate
  • Survival of one extra pig per sow has a value of 33 Euro
  • Reliable ventilation and alarm systems are essential as the pigs can die within 20-40 minutes if the ventilation system breaks down

 

Daily gain and feed conversion ratio

When the temperature is above comfort level the pigs eat less. Daily gain varies between 600 and up to more than 1000 gram per day for growing pigs (30-110 kg) and it can easily cost 200 gram per day if the farmers do not have advanced ventilation and have to raise pigs  in for instance temperatures of 30 Celsius or even higher.

https://www.agric.wa.gov.au/summer/heat-stress-pigs

Also the feed conversion ratio can be reduced with up to 20% if the pigs are raised in high temperatures. These numbers are so crucial, so if the farm companies want to produce meat for the world also in the future this requires advanced ventilation.

Even in a country like Denmark, where it is relatively cold and all farmers have advanced ventilation, a collection of production results from 43 farms showed that the daily gain was 50 g less in July compared to January. So the pigs grow more quickly during winter even though the air quality is worse. That illustrates that even advanced ventilation systems can be improved.

The economic production benefits change from day to day due to variation of meat prices, feed prices etc, but a report from August 2016 in Denmark shows that if the daily gain in the finishing unit (30-110 kg) changes +/- 100 gram/day. The value for the farmer will be up to +/- 1.7 Euro/pig (12.6 dkr/pig).

http://vsp.lf.dk/Publikationer/Kilder/Notater/2016/1617.aspx

Facts

  • When pigs grow from 30-110 kg daily gain on farms around the world the daily gain is typically varying between 600 and 1000 gram/day
  • Heat stress can easily reduce the daily gain with 200 g/day and feed conversion ratio can be reduced up to 20%
  • +/-100 gram in daily gain cost +/- 1.7 Euro/pig

 

Fertility

A farmer in Brazil has seen the advantages with advanced ventilation when they want the sows to get pregnant. The farmer had one house with cooling pads and tunnel ventilation and another simpler house with curtains and circulation fans. Apart from the ventilation set up, the houses were identical. In the house with advanced ventilation it was easier for the sow to get pregnant. The farrowing percentage grew 6 percent point from 86% to 92%.

If it takes longer time for the sows to get pregnant the farmer has to spend more feed per pregnancy and the sow will get fewer piglets per year. In Denmark the value is 11.7 Euro (88 dkr) for each percent point the farrowing percentage changes.

Facts

  • It is more difficult for a sow to get pregnant if it has heat stress
  • In Brazil the farrowing percentage was improved by 6 percent point in house with advanced ventilation
  • In Denmark the value is 11.7 Euro for each percent point the farrowing percentage change

Voimmeko auttaa?

Palaa etusivulle
Valitsemalla hyväksyt meidän evästeet

Virheellinen käyttäjän tunnistaminen

Jokin meni väärin, yritä myöhemmin uudelleen

Virheellinen käyttäjän tunnistaminen

Jokin meni väärin, yritä myöhemmin uudelleen