Biz uzamanlarız

Mesajı gönderirken bir hata oluştu; lütfen daha sonra tekrar deneyiniz

Bir soru sorun

CS_Mine shaft_Hero_845x475.jpg

Developing a customised ventilation system solution

Cold weather provides a unique set of problems to the efficient operation of equipment and processes, whether land-based, offshore, or marine. To optimise inside temperature and humidity it’s vital to achieve and maintain a constant, dependable supply of air from the outside – no matter the weather.

Water droplets from ventilation fans freeze in winter

A US Mine Engineering company contracted Munters to resolve a water carryover issue on the discharge side of the mine shaft ventilation fans. Water droplets entrained in the mine shaft ventilation air were being discharged out of the fans. The liquid would freeze in the winter on all surfaces in a large radius around the exhaust fan creating a dangerous situation as the liquid froze. It would also coat nearby equipment, creating potential maintenance and operating concerns. Additionally, this liquid could contain contaminants that could mix with groundwater.

Developing and installing a customised system

Munters developed a separator system that was engineered and manufactured to capture entrained liquid. The equipment consisted of:

Munters DH Series mist eliminators

Housing with transition to attach to the discharge side of the fan

An inlet wash system to wash off any insoluble particulates that may coat the chevrons

Uptumed discharge section to vent the air straight up

Hızlı greçekler

  • Ensuring adequate air supply at all times
  • Protecting processes and equipment
  • Stopping build-up of bacteria and mold
  • Reducing maintenance requirements