Biz uzamanlarız

Mesajı gönderirken bir hata oluştu; lütfen daha sonra tekrar deneyiniz

Bir soru sorun

All-in-one solution - Helping poultry producers increase farm profitability

Heat Recovery Solution

With rising energy costs, and increasingly severe climate conditions, many poultry farmers are considering investing in heat exchangers as a way of cutting their bills. But lower energy bills aren’t the only benefit of heat exchanger solutions. This is really an all-in-one solution that helps you to ensure optimal conditions in farm facilities, while respecting the surrounding environment.

Energien i den opvarmede luft fra stalden anvendes til at opvarme friskluften når den passerer gennem Munters genvindingsrotor i Heat-X Rotate.

Heat-X Rotate er helt unik i markedet, idet den er selvrensende. Rengøring foregår helt automatisk ved hjælpe af luftkompressor og dyser. Du skal med andre ord ikke bruge din tid på rengøring eller bortskaffelse af vaskevand.

Hvis du er klar til at træde et skridt fremad i dine bestræbelser på at forbedre bedriftens samlede miljøaftryk og bundlinje, så har Munters den rette løsning til dig.

Download produktinformation

Innovative Heat Recovery that helps poultry producers save money

The production potential of a chicken farm can only be fully achieved if ideal conditions in the indoor microclimates are met. This requires sufficiently energetic air ventilation systems.

At the same time, energy saving is one of the most urgent priorities for farmers, given rising energy prices and the significant share of the energy component in the cost of poultry products. 

Calculate your annual savings HERE

 

Udfordringer for fjerkræproducenter

Når luftskiftet sænkes for at spare strøm og varme, så lider dyrene under dårlig luftkvalitet, øget luftfugtighed, øget CO2 og NH3 koncentration, samt øget støvmængde.

Det er ikke et sundt miljø for dyr og mennesker

I stedet kan du udnytte den tunge og varme staldluft til at forvarme friskluften og dermed øge din minimumventilation om vinteren uden at det koster ekstra på energiregningen og uden at du kompromitterer kvaliteten af strøelsen. Stadig flere fjerkræproducenter har installeret varmegenvinding for at få glæde af disse fordele. Uanset om du opdrætter kyllinger eller producerer æg, så vil du øjeblikkeligt opleve en stor forandring efter installation af Munters Heat-X Rotate.

Who is already changing the way they farm?

Many farmers have already installed the Heat-X Rotate, and the benefits have been tangible right from the start. It has increased the profitability of the entire farm, while ensuring a healthy and comfortable environment for the animals, as well as protecting the surrounding environment (thanks to the reduction of CO2 due to heat energy savings).

“The first batch of chickens has now been in the barn, and they seem to be having a great time”

Hans Klemmensen –Operations Manager - KJ Klimateknik

Discover the success story of one of Denmark’s leading producers who decided to install a heat recovery system in his stables.

 

heating-unit_heat-x-rotate_scene (1159x1200).png