Wij zijn experts

Er is een fout opgetreden bij het verzenden van het bericht, probeer het later opnieuw

Stel een vraag

CELdek_Mi_T_Edg_with_logo_on_side_web.png

CELdek evaporative cooling and humidification pad

The original quality pad from the original manufacturer, certified GREENGUARD Gold

Why should you choose Munters CELdek®?

It stands as one of Munters' pioneering technologies dating back to the 1950s, enduring for over 60 years and consistently advancing through improvements by the Munters Research & Development team. It has evolved into the benchmark for evaporative cooling pads in the market.

The paper used in CELdek is a thin specialty-grade paper, exclusively developed for Munters. The result is that CELdek wets faster than any other pad on the market. Faster wetting means immediate cooling and potentially less system run time, saving you water, energy and money.

If the pad does not dry completely, it could break down from the inside out, reducing the life of the pad. As an added precaution, CELdek is chemically treated to resist deterioration.

For extra demanding environments, Munters has developed MI-T-edg® coating, which is considered to be the strongest most weather-resistant edge coating available and is the only edge coating with patented algae resistance.

This means that extending the lifespan of your evaporative cooling pad by just two years can lead to significant cost savings. When you invest in CELdek, you benefit from decades of research and development, along with the expertise of engineers knowledgeable in ventilation systems and the scientific principles that define a high-quality pad.
 
GREENGUARD Gold certification

As of January 1, 2015, Munters CELdek evaporative cooling and humidification pads have been tested for emissions from over 360 individual chemicals of concern, guaranteeing them as having non-harmful emissions. We are the only GREENGUARD Gold certified manufacturer of cooling and humidification media by UL Solutions, the developer of the most stringent product emissions standards in the world. Yearly testing of the products is required to maintain the certification.