Somos expertos

Ha ocurrido un error cuando se ha enviado el mensaje, por favor, inténtelo más tarde

Haz una pregunta

VX-Fan-in-a-farm.png

VX fans in China

The VX fan series is Munters premium exhaust fan line, which has been widely used around the globe, especially in swine and dairy applications.

Our engineers understand the harsh environment in which VX fans must perform and have designed the series to optimize both performance and quality. The parts and components withstand corrosive gases from the internal environment as well as sunlight and heat from the external environment, making VX the benchmark for our industry.

Working together with the other ventilation products of Munters, VX fans can accurately maintain the proper balance of indoor temperature and air quality to ensure consistent production levels, maximize feed conversion, lower mortality rate and improved conception rate.

In China the interest for VX fans is booming. “We see in July 2016 (compared to 2013) a doubling of installations of the VX fans and we estimate to have a fourfold of number of installations when 2016 is completed”, says Product Manager Kane Liu.

Munters ventilation system has been adopted by the advanced farms in China with an ever-increasing demand. In recent years, China’s livestock industry has put priority on developing large-scale farming and building modern breeding system, and thus, brings huge opportunities to the high-performance Munters solutions.