Wir sind Experten

Beim Versenden trat ein Fehler auf, bitte versuchen Sie es später erneut

Fragen Sie uns

Green  Dry Product_web.jpg

New Arrival Phase II of GreenDryTM Series Dehumidifiers

Feb 2, 2016

Remarkable “Made in China”

On 21st August 2015, new arrival Phase II of GreenDryTM, which was independently developed by AirT China, officially launched. Compared with the units of Phase I, the upgraded units are more customized. Beyond that, the industry leading Super DH, LDP (Low Dew Point) and PP (PowerPurge) units are also provided as options. GreenDryTM can create a production environment with stable humidity as well as minimized energy consumption even under very harsh working conditions. 80% of GreenDryTM series have launched up to now and the final phase will be released at the end of this year.