Vi er eksperter

Der opstod en fejl under afsendelsen af beskeden, prøv igen senere

Stil et spørgsmål

CIBSE1936_Banner_350(w)x250(h)221.jpg
nov 26

CIBSE Build to Perform

nov 26 09:00 - 17:00

Munters is delighted to be exhibiting at CIBSE Build to Perform Live 2019, which will take place 26-27 November at London Olympia. Focusing on engineering a better user experience and improving productivity of building users, CIBSE Build2Perform Live 2019 will see over 200+ visitors, 70+ exhibitors, and hear from over 130+ speakers.

On the Munters stand 221, our expert Service team will be talking about the benefits of using the latest EC fan technology to upgrade and refurbish AHU's. These benefits include:

  • Significantly improving energy efficiency
  • Enhancing operational reliability and resilience
  • Reducing noise 

By choosing to refurbish your old AHU, you will benefit from similar running costs (compared to new) without the higher install costs, with faster installation and less disruption. 

Proven in a range of industries including airports such as Heathrow, Luton and Birmingham, plus offices, hotels, swimming pools and more. 

Register for FREE at CIBSE Build to Perform or learn more about the event.     

Follow on social media @CIBSE #Build2Perform

More about AHU upgrades

Events

  • SEP25

    09:00

    12th Northern Bavarian Drinking Water Conference

    The drinking water conferences, which now take place in five venues in Germany, are aimed at employees of municipal water suppliers, engineering…

  • DEC03

    09:00

    Meistererfahrungsaustausch

    The "Meistererfahrungsaustausch 2024", an exchange of experience between the masters of water supply companies and pipeline construction companies,…

  • JUN03

    11:00

    The Battery Show Europe

    The Battery Show Europe provides an opportunity to source the latest manufacturing solutions from across the battery supply chain for industries…