Dovolte, abychom vám pomohli

Při odesílání zprávy došlo k chybě, opakujte akci později.

Položit otázku

CS_Cold cosmetic storage_Hero.jpg

Munters Icedry®800 eliminates ice and snow in cold storage

Dr. Suwelack Skin and Health Care AG processes animal products into cosmetic raw material. One of the end products for the company’s raw material is dermatological face masks.

From production straight into the cold storage

Plates of collagen are made first when producing face masks. The product goes directly into -25C cold storage after solidification in the sheet production machine. The machinery for subsequent production steps is located inside the cold storage area to ensure high product quality and consistency.

The production process encountered a significant problem during the regular transport of finished collagen sheets from the production area into the cold storage area.

Since the production area was warmer and more humid the movement of the product tracked in a significant amount of moist air upon entering the cold storage area. When this infiltrating moisture hit the cold surfaces inside the cold storage area it quickly turned to ice and frost throughout the entire cold storage area
(at doors, on evaporator fins, on production machinery, etc).

As a result, facility personnel regularly had to defrost the cold storage area, disrupting production and increasing maintenance costs.

The Munters solution

This issue was solved by installing a Munters Icedry®800 inside the cold store. Air from the cold store was recirculated through the IceDry800, dehumidified and blown down the two door openings like dry air curtains.

The cold storage area is now free from ice and snow thanks to the Munters IceDry 800. Production and storage are now free from moisture-related problems.

Stručná fakta

  • Reduces ice formation
  • Cuts down on time-consuming and costly defrost cycles
  • Saves energy and reduces maintenance
  • Reduces the risk of damaged products
  • Eliminates the risk of worker injuries